6/3/2010 12:06 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Basically would be difficult to build aplication which will communicate with LOGO! PLC. Look at LOGO! PLC driver based on LabVIEW and LOGO! +KNX(Control panel for LOGO! ) Perhaps could give you some ideas. My suggestion is to go with ""hgher" typr of CPU.... Good luck! Best regards, Hristo Mihalev |
6/3/2010 2:14 PM | |
Joined: 10/7/2005 Last visit: 9/4/2025 Posts: 3049 Rating:
|
Hello rllabres you can find an English version of an Excel based Logo Data Logger HERE. The original German versionwas developed by Superbrudiand can be foundHERE. Tailor1986 then took Superbrudi's logger and added a VBA based Visualisation to it which you can find HERE(and which just so happen to be a visualisation of a central heating system). While I wouldn't call it a "SCADA" and don't know if it is what you are after, it may at least point you in the rigth direction and act as a starting point as well asshowing that "backyard" development is alive and licking in the Logo community (andeven if you don't speak German, you should be able to get the gist of the German version if you use an online translation). I hope this helps |
Cheers |
|
This contribution was helpful to
1 thankful Users |
Follow us on