Default Header
(header konnte nicht geladen werden)
3/5/2007 4:02 PM | |
Joined: 9/13/2005 Last visit: 5/28/2025 Posts: 86 Rating:
|
Hi, did you already have a look at following FAQ? http://support.automation.siemens.com/WW/view/de/22232559 When you set SELFCOMP=0 at your SFC it will wait at the end of the SFCs RUN sequenzer until it receives the COMPLETE command from SIMATIC Batch. In your Batch recipe you just have to syncronize your phases with a sync line. Doing this Batch will wait until all phases connected with the sync line signalize that they are ready to complete(READY_TC) and then sends the COMPLETE command to all phases (sfc). |
Best Regards - Mit freundlichem Gruß - yoroshiku onegaisimasu - Sincères salutations |
|
Follow us on