3/9/2021 10:46 AM | |
Posts: 2 Rating:
|
Hello everybody, Today I am facing a problem with S5 PLC 135U. As in topic I am attaching iStack screens. I am not so familiar with S5 diagnostic, would somebody could tell me which peripherial remote IO (address) seems to be fualty? Basically we are having problems while we are powering up a machine. After few seconds PLC is going into stop mode and ADF and BASP LEDS are constant ON and RED, STOP is blinking red slowly. After few minutes stop/start from CPU switch is helping and machine is ready to work. From what I've read on forum, I am assuming that machine may have problem with one of the remote IO. CPU have cards: 2x 6ES5 432-4UA12, 2x6ES5 451-4UA12, 1x6ES5 470-4UA12 and communication module : 6ES5 308-3UC11. and 13 ET200B Remote I/O Correct me if I am wrong, but I am assuming that ADF fault is coming from OP-REG: 53AC - Instruction T IW/QW 172 ? So probably I am having issue with remote IO which cover address 172? Do I think correctly? I would appreciate if somebody would explain me more attached iStack and possible causes of stop and also correct me if I am wrong. Attachments5_135u_istack.zip (670 Downloads) |
Follow us on