2/12/2021 9:23 AM | |
Joined: 3/6/2019 Last visit: 5/18/2024 Posts: 12 Rating: (0) |
I have configured a devices withS7-1212 DCDCDC, Siwarex wp231 module, KTP 400 Hmi and loadcell. I have used *READY FOR USE LEGAL FOR TRADE * file from Tia portal forum...Ready to use S7. Zip https://support.industry.siemens.com/cs/in/en/view/66825585 This file....... I have loaded the program through Tia portal v15 and calibrated with weights. I have configured using siwarex manual and till the end it was nice they are showing weights perfectly and it worked..... But after some days they behave like anything.. They are not showing weight and load cell is perfectly alright and module is alright So I went through monitering of program online it's not showing in online mode also from module. Where the weight displays in address. It's empty there between "" "". The one thing I have did is Reset the PLC and started again it worked again.... But again after some days it's repeating with same it's not showing weight.... Even 0 is also not showing on HMI display.. But this problem is repeating again and again... After few days... I'm attaching 📎 image of HMI display where weight appears.. After problem exists. Please help me to get rid of this problem.... |
Last edited by: Sai Teja at: 02/12/2021 09:25:00Last edited by: Jen_Moderator at: 02/12/2021 12:17:41Optimized link. |
|
11/19/2023 12:03 PM | |
Joined: 3/6/2019 Last visit: 5/18/2024 Posts: 12 Rating: (0) |
It solved ,I didn't used the data logging yet |
This contribution was helpful to1 thankful Users |
Follow us on