5/10/2017 10:53 AM | |
Posts: 3 Rating: (0) |
Hello, I have a problem compiling with Eclips C++ and IoT2040 SDK 2.1.3, when I add a separate file the compiler does not compile correctly. build file in alphabetic order Attach sample project for example In the project I have the following files aClass.cpp aClass.h example.cpp serCom.cpp serCom.h In this case Info: Internal Builder is used for build i586-poky-linux-g++ "i SDKREFERECE" -o aClass.o "..\\aClass.h" i586-poky-linux-g++ "i SDKREFERECE" -o aClass.o "..\\aClass.cpp" i586-poky-linux-g++ -lmraa -fno-use-linker-plugin "--sysroot=SDKREFERECE" -o Prova3 aClass.o SDKFOLDER\ i586-nlp-32-poky-linux/usr/lib/../lib/crt1.o: In function `_start': if remove aClass.xx files build and link example.cpp correctly, but error occur on serCom if remove serCom.xx file build and link examples.cpp correctly and generate executable file How to solve that problem? any idea? AttachmentProva3.zip (239 Downloads) |
Follow us on