7/2/2023 11:24 AM | |
Joined: 3/31/2023 Last visit: 9/15/2024 Posts: 25 Rating: (1) |
In my Node-red flow, i am taking data from Siemens PLC through OPC-UA node in node-red. I'm getting data perfectly for some-time(meaning whatever changes i make in Tia portal program is also shows in node-red debug window.[Refer to screenshot -1]). But after certain time(2-3 minutes), whatever changes i made at Tia portal program does not reflected back in node-red debug window[Refer to screenshot -2]. I don't know why? Also, OPCUA node status is also changing from "'Active subscribing' to 'keep-alive' to 'active subscribing'..........[Refer to screenshot -3]" I am using * Tia portal[Siemens V16] * PLC sim advanced V2.0 * Node-red(windows 11) * OPCUA contrib node(but not IIOT OPCUA node) Those who need my-node-red flow, i have pasted it here.
Attachmentscreenshots&flow.zip (549 Downloads) |
Last edited by: Jen_Moderator at: 07/03/2023 11:07:56NodeRed Flow added as .txt file. |
|
7/3/2023 11:17 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject Error --- " [31m Client node error on: error: [" error at active reading: Transaction has timed out ( timeout = 15000 ms , request = Read Request)"] [39m" is published within the conference IOT2020 / IOT2040. Jen_Moderator |
Follow us on