11/13/2018 9:50 AM | |
Joined: 10/18/2017 Last visit: 3/11/2024 Posts: 26 Rating:
|
Hi guys, (CODE and SS in the link) I have a question that so far i have not been able to answer myself. I have a S7-200 PLC, with CP243 Ethernet Module, and a KTP700 that i want to use as a local OP, via the ethernet port in the CP243. So far what i have done is: - Run the module configuration wizzard with the settings that you can see in the link. - The wizard finishes ok and generates ETH0_CTRL - I called the ETH0_CTRL block in my main routine, and it finishes ok as well, with code 1(ready), and no error messages. - I created a DATA BLOCK in the S7-200 PLC and pasted the 3 values that i care about there. (VD18, VD20, VD22) - I created a project in TIA v13, there i added a KTP700 and defined a connection using the S7-200 DRIVER, and setting the ip of connected device to (192.168.123.97 - lan module ip). - I created a tag in the HMI< with the memory adress VD22, and tied it to a I/O field on the main screen. - After the HMI runtime starts, a short message stating: "Connection dissconnected: Station at adress 192.168.123.97, rack 0, slot 0." and the field just shows ######. I am really intrigued as to why i cannot display the value on the HMI, as i can program the PLC via the ETHERNET module just fine. Also, i need to mention, that when trying to upload to the PLC i get a warning saying i need to reposition the inteligent modules, or something along those lines. Any help would be greatly appreciated, as the client doesn't want any other display or PLC solution :(( Below i attached the: MicroWin project for the PLC Tia V13 hmi project Screen shots AttachmentScreenShotsMicroWin.zip (656 Downloads) |
Last edited by: Promotor at: 11/13/2018 9:52:59 AMLast edited by: Jen_Moderator at: 11/14/2018 6:22:09 AMRemoved link and added file as an attachment. |
|
11/13/2018 1:40 PM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating:
|
Hello, and how you expect that Remote TSAP as 10.00? In some documentation is recommended set 02.00 for remote Client device. Try set this value and reconfigure again ETH Wizard, download, test. Update: what is your CP-243 position on S7-200 cfg? Due that recommended position. You check that Automatically (something going to me that this apear in cfg)? Update2: here is mentioned FAQ (it can be helpful): How you configure connection with WinCC RT or WIN based HMI |
Last edited by: Duris_I at: 11/13/2018 1:45:41 PMLast edited by: Duris_I at: 11/13/2018 1:46:24 PMLast edited by: Duris_I at: 11/13/2018 1:53:14 PMLast edited by: Jen_Moderator at: 11/13/2018 2:14:48 PMOptimized link. With best regards... |
|
This contribution was helpful to
1 thankful Users |
Follow us on