7/14/2017 12:58 PM | |
Joined: 5/22/2014 Last visit: 4/17/2018 Posts: 32 Rating: (1) |
Hi guys! I'm trying to program in C++ following the 'Getting Started.pdf' so i'm using Eclipse for C/C++ developers. The problem is that i want to use the Snap7 library but i can't import or install the library, can you help me with it? My OS is Windows10. Thanks you all. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/17/2017 12:59:24 PMNew subject after splitting |
|
7/17/2017 9:21 AM | |
Posts: 215 Rating: (6) |
Have a look here. In the second post, bergmanu says something that might proove helpful. |
7/17/2017 9:33 AM | |
Posts: 37 Rating: (3) |
The easiest way is to use scp (e.g. WinSCP on Windows). Michael |
7/18/2017 9:20 AM | |
Joined: 5/22/2014 Last visit: 4/17/2018 Posts: 32 Rating: (1) |
Hi again, i'm trying to set the snap7 library as explained here: Snap7Sourceforge The problem comes when i have to find this path: \iss-iot-win\devkit-x86\sysroots\i586-poky-linux\usr\lib On my installation i dont have this one, as you can see in the photo. Ideas how to fix it? |
10/19/2017 6:57 AM | |
Joined: 6/19/2017 Last visit: 6/28/2024 Posts: 8176 Rating: (169) |
New question published by techniker0815 is split to a separate thread with the subject Error occurs bei Build after included the snap7.h. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on