1/16/2007 10:41 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
Hi Danielle, OPEN MODBUS TCP is a protocol you may use with the CP 343-1 and the CP 443-1. How can you establish OPEN MODBUS / TCP communication via the CP343-1 or CP443-1 and where can you find further information? If this is working is only to say if the functioncode that is possible with this driver is also possible with the system you want to couple.... [:o] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on