4/9/2024 10:09 AM | |
Joined: 5/25/2020 Last visit: 5/31/2024 Posts: 3 Rating: (0) |
Hello everybody, I'm currently trying to use 6 monitors on 1 PC but when I try to set the "monitor number" TIA limits me to setting only 4 monitors. I'm pretty sure TIA itself doesn't allow me to use more than 4 monitors but it would be really nice if somebody could confirm this for me. I did find this older topic: WinCC Professional : Division of a screen on 6 monitors This acknowledges that more than 4 monitors is not possible in TIA V14 but I would like to know if this is something that has been changed in TIA V16. Hopefully somebody knows a bit more about this. Thanks in advance! |
4/9/2024 11:10 AM | |
Joined: 5/30/2022 Last visit: 5/30/2024 Posts: 524 Rating: (86) |
Hi Nick Forum, I'm afraid the limitation continues with the current versions. The maximum number of monitors to be configured is 4 on a WinCC Professional. But you can try splitting a screen into multiple monitors, check out the following FAQ: How do you use multiple monitors simultaneously with the WinCC (TIA Portal) Runtime Professional? |
If this information really helps, you could use the Rate function. |
|
This contribution was helpful to1 thankful Users |
Follow us on