7/14/2025 1:24 PM | |
Joined: 8/3/2009 Last visit: 9/19/2025 Posts: 16457 Rating:
|
Hello Kevic I´m no sure if it could make problems if you use this combination (Win11 and TIA V15.1). In the Compatibility tool this is not released. Only since V17 there is a release for Windows 11 https://support.industry.siemens.com/cs/de/en/view/64847781 And you should at least also use the latest updates for your V15.1: https://support.industry.siemens.com/cs/de/en/view/109763890 Bye Murof |
If this Information really helps, you could use the Rate function |
|
7/15/2025 9:42 AM | |
Joined: 8/3/2009 Last visit: 9/19/2025 Posts: 16457 Rating:
|
Hello Kevic One thing I noticed in the past, if you go online to HMI devices and then try to download the program to the HMI this could lead to problems/issues. In case of an HMI transfer you should go offline or deactivate all online connections first and then do a "Extended download to device " Check also this FAQ for another way to transfer: https://support.industry.siemens.com/cs/de/en/view/109740696 Bye Murof |
Last edited by: Murof at: 07/15/2025 09:44:35If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on