2/28/2021 2:18 PM | |
Joined: 9/24/2013 Last visit: 5/6/2025 Posts: 36 Rating:
|
Hello. Seems that the problem is somwhere elese. The network 1 works fine with no errors, and when the network 2 starts it gives info about wrong data lenth and so one. There are only ATV320 inverters in the system, so the data is exaclty the same. I add an attachement with most important parts of the program. I didnt added screens of all the triggers and all the MODBUS_MASTER calls , but the idea is the same , i did 5 times check of the double modbus master triggerring, i didn't found nothing. If theres one condition which I have found and have no idea how to solve when MODBUS_MASTER instances are called the same time for different CM PTP the system goes crazy. I'm trying to figure out why ;) . AttachmentModbus RTU Config 1.zip (640 Downloads) |
Follow us on