1/16/2025 8:15 AM | |
Joined: 11/13/2024 Last visit: 3/20/2025 Posts: 1 Rating:
|
Hello! I am trying to connect my S7-1200 to TCSB through CP 1242-7, but it fails to connect to the server. I followed [the embedded] video tutorial, and also the tutorial from this and this, but to no avail. I have a connection to the mobile network, but in TIA, inside online&diagnostics in the partner tab, connection to the partner shows to be disconnected. I checked the SIM in my mobile phone and it appears it doesn't have a mobile number, although I can access the internet. I am certain that my PC is properly configured to use TCSB, as I can see the port (55097) open when checking it with canyouseeme.org. I use a 1214C AC/DC/RLY V4.3.1 (6ES7 214-1BG40-0XB0) with CP 1242-7 V2 GPRS V3.3.32 (6GK7242-7KX31-0XE0). In TIA portal -> online & diagnostics on the CP -> protocol diagnostics I can see the [attached] logs. Can it be the CP not connecting to 3G/4G network but only to 2G? Does RemAddr refer to the remote server's IP? Meaning it tries to connect to the address 0.0.0.0? (although I configured the IP in CP's settings) Can someone see the problem from the CP logs? Attachment16.01. protocol diagnostics.txt (135 Downloads) |
Last edited by: Moderator_Lan at: 01/16/2025 10:03:22Links optimized / Video embedded / Code attached / Image embedded |
|
Follow us on