8/12/2010 2:50 AM | |
Posts: 64 Rating:
|
I have a “S7-313C” station connected to “OP17” via MPI. I connected a programming device to the CPU and upload the S7-station to the PG.(according to the attachment) But when I want to upload the op17 to the PG, “no connection error “ is appeared. I should note that, I can see both stations (S7 and OP17) in accessible nodes, one with MPI add=1 (OP) and another with MPI add=2 (CPU). Connection to CPU established without any error, but connecting to OP is failed. What’s your solution regarding this problem? Sincerely Mazdak AttachmentOP17 Config.pdf (523 Downloads) |
8/12/2010 9:22 AM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, To make backup of OP17 (upload) is possible only using Prosave.(How do you backup/restore with a Windows-based panel? ). And you will need Seriell RS232 (6XV1440-2K..) cable. (pins assignment - http://support.automation.siemens.com/WW/view/en/29034071 ) Best regards, Hristo Mihalev |
8/12/2010 9:24 AM | |
Joined: 4/24/2006 Last visit: 9/15/2025 Posts: 9027 Rating:
|
Dear mazdak, When you want to upload the program from OP17, you will need Prosave. Probably it is installed on your PC, otherwise you can download here: Service Tool ProSave v7.4.4 To communicate with OP17, you can only use Serial connection You will need the cable 6XV1-440-2KH32 Here a link, with pin connections: What is the serial cable assignment for transferring the configuration to an RMOS operator panel? Best regards, Wizard |
Last edited by: Wizard at: 8/12/2010 9:25 AMI typed too slow ;-)) |
|
This contribution was helpful to
1 thankful Users |
Follow us on