12/23/2024 3:17 AM | |
Joined: 7/10/2024 Last visit: 12/31/2024 Posts: 1 Rating:
|
I am experiencing an issue while attempting to connect my PLC to the LOGO! Soft Comfort software. Despite multiple troubleshooting attempts, I keep encountering the error message:"Unable to access the remote device." Details of my setup:
I have verified the following:
Despite these confirmations, the software fails to establish a connection and continuously shows the "Unable to access the remote device" error. Could you please assist me in resolving this issue? If further diagnostics or specific steps are needed, I am happy to provide additional details ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 12/23/2024 09:36:41New subject after splitting |
|
12/23/2024 3:03 PM | |
Joined: 5/6/2022 Last visit: 9/9/2025 Posts: 589 Rating:
|
Hi Ahmed Mubarak, I have been reviewing the documentation and I think the problem has to do with LOGO! PLC Model. The device with part number 6ED1052-1MD08-0BA2 that you are trying to connect to, can only be configured using LOGO!Soft Comfort V8.4 or higher as you can see in the product description in the following link: Therefore, in this case I would recommend you to update your LOGO! Soft Comfort software to V8.4 from the link below: In principle with this upgrade you will be able to communicate and you will no longer have this error. Best regards!
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
7/10/2025 3:00 PM | |
Joined: 12/18/2014 Last visit: 9/10/2025 Posts: 35947 Rating:
|
If you mean this link: Firmware update for LOGO! 8.4 basic devices and service pack 1 for LOGO! Soft Comfort V8.4 |
This contribution was helpful to
2 thankful Users |
7/17/2025 3:41 PM | |
Joined: 7/17/2025 Last visit: 7/17/2025 Posts: 1 Rating:
|
Sorry firmware update gedownload maar wat moet je dan doen? mvg Alex |
Follow us on