7/27/2023 6:09 AM | |
Joined: 3/25/2015 Last visit: 8/5/2025 Posts: 124 Rating:
|
Hello I'm having problems with a 4Gb non-Siemens usb stick not being recognized by the HMI KTP700 Basic. The usb stick is working fine on every pc I plugged it in. Even on a TP1900 Comfort. Is there a minimum required size required for KTP700 to be able to recognize it? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/27/2023 11:17:25New subject after splitting Kind regards |
|
7/31/2023 11:17 AM | |
Joined: 8/3/2009 Last visit: 9/4/2025 Posts: 16343 Rating:
|
Hello simonspt No I think there is nothing damaged on your device. We tried also different USB Devices on our Basic Panels 2nd Gen. Only a few worked also in our tests. I have also different sticks that works (2GB, 16 GB...). Here are the specifications for the USB Recovery: https://support.industry.siemens.com/cs/de/en/view/109744950 But the USB Stick from Siemens that is released as accessory is also a 32GB with USB3.0 ... so I´m not 100% sure what are the definitiv criteria for a working one... but Siemens Stick should work bye Murof |
If this Information really helps, you could use the Rate function |
|
6/16/2024 2:59 AM | |
Posts: 1 Rating:
|
Thank you very much Simonspt, the same thing happened to me with my KTP700 BASIC HMI, with the 2GB USB it did not work, when using the 16GB it worked perfectly. |
Follow us on