5/17/2021 11:59 AM | |
Joined: 3/30/2020 Last visit: 9/15/2025 Posts: 5450 Rating:
|
Hello. The S7-1200 HSC that uses onboard inputs, Special instructions are used to control the HSC, as mentioned by Mr Marcjan on another topic. The system manual for the S7-1200 explains the HSC workings: Application example: |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
2 thankful Users |
5/18/2021 8:22 AM | |
Joined: 1/18/2020 Last visit: 7/2/2022 Posts: 53 Rating:
|
Thanks for all of your response, I appreciate it. I see that there's a lot to consider when using a high-speed counter and converting the program from s7-200 to s7-1200. No direct conversion for this. You must need to add OB40 (Hardware interrupts) You need to define HSC in S7-1200 Controller Properties. - Enable HSC - You need to determine the ff.: - Type of counting - Operating phase - Configure the Digital inputs I'm really not familiar with the high-speed counter-programming Can you have a look at my s7200 backup program? Just change the extension file from .docx to .rar. Thanks in advance AttachmentSUL A (1).docx (654 Downloads) |
5/21/2021 7:49 AM | |
Joined: 4/22/2010 Last visit: 3/31/2025 Posts: 5697 Rating:
|
Hello, In TIA you just have to place one block what can do the same. See S7-1200: Application Examples for High-Speed Counters (HSC) Regards, Marcjan |
Problem solved? |
|
This contribution was helpful to
1 thankful Users |
Follow us on