8/3/2006 6:41 AM | |
Posts: 23 Rating:
|
Hi Late, Thanks, I created cfg file, but can you guide me how to open it in CA01 off line mall in detail. Regards, G. Swaminathan |
8/4/2006 11:49 AM | |
Posts: 23 Rating:
|
Hi, Pl. find the attachment test.zip for a sample Hardware file exported in cfg format. Kindly letme know how to create BOM with this. Thanks Swaminathan Attachmenttest.zip (803 Downloads) |
8/6/2006 3:23 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="swaminathan"]Please find the attachment test.zip for a sample Hardware file exported in cfg format. Kindly letme know how to create BOM with this. Hi Swaminathan, I have made a document with the hole import and description for you and of course also for the other members of this forum. Please consider that the CD I used was not the newest one and also have not the same structure as in your country. The CA01 comes more times a year on CD and is updated in June I believe, I haven't a new one yet, the wizards are all the time better and better. If you like it this way, please let me know... PS. I have put the Black and White pdf on the Forum because the Fullcolored one was something to big, if you want also the colored one, please write me a Private Message with your email-address and I will send it to you. AttachmentThe exported installation from the Hardware configuration in the Mall BW.pdf (929 Downloads) |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
This contribution was helpful to
1 thankful Users |
8/7/2006 6:47 AM | |
Posts: 23 Rating:
|
HiLate, Thank You very much for the reply. It wasvery much Useful. But I tried to create BOM for ET200M remote station with S7-400CPU, where I could not get the BOQ for remote stations. Only main rack part numbers alone are listed out. Herewith I attached the cfg file. Best Regards, Swaminathan Attachmentkunkel.zip (765 Downloads) |
Last edited by: swaminathan at: 8/7/2006 12:27 PM |
|
8/12/2006 3:30 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="swaminathan"]Thank You very much for the reply. It wasvery much Useful. But I tried to create BOM for ET200M remote station with S7-400CPU, where I could not get the BOQ for remote stations. Only main rack part numbers alone are listed out. Herewith I attached the cfg file. Hi Mr. Swaminathan, Because you have a older version of STEP7 {V5.3 + SP2 + HF2} and maybe never updated your catalog in STEP7 {HSP = Hardware Support Package}, there are placed older cards. Those are asked for when importing in the CA01 and then you have to give up the newest ones. AttachmentThe exported installation from the Hardware configuration in the Mall 2.pdf (811 Downloads) |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
This contribution was helpful to
1 thankful Users |
8/14/2006 5:58 AM | |
Posts: 23 Rating:
|
Hi Late, Thank You, I will update my Simatic manager and CA01.[:D] Regards Swaminathan |
8/16/2006 8:56 PM | |
Joined: 1/7/2006 Last visit: 5/11/2025 Posts: 2705 Rating:
|
[quote user="swaminathan"]Thank You, I will update my Simatic manager and CA01. Hi G. Swaminathan, No thanks, I'am glad I could help you..[:D] Have you already updated your STEP7 V5.3 to SP3: Service Pack 3 for STEP 7 V5.3 and STEP 7 Professional Edition 2004{220Mbyte} Or do you want to update to V5.4[:P] And the HSP: Hardware Support Packages (HSPs) How can you update the hardware catalog without direct Internet access? |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on