10/14/2024 2:08 PM | |
Joined: 9/21/2024 Last visit: 5/14/2025 Posts: 8 Rating:
|
Hello friends I want to directly enter the Siemens HMI settings( KTP1200 basic) , but the panel enters the program as soon as it is turned on, and I have not defined any icon to go to the settings page in the program I have written, I was working on the smart server settings, which unfortunately I can't connect to the panel through Tiaportal!!!! Can you guide me? Best Regards Navid ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 10/15/2024 12:30:48New subject after splitting |
|
10/15/2024 1:48 PM | |
Joined: 2/17/2020 Last visit: 8/29/2025 Posts: 1251 Rating:
|
Hi, The Startup / Autostart option must be set to 0 seconds, so the Runtime program starts as soon as you turn on the HMI device. You can try to do a backup through ProSave to save the project before resetting the HMI device to factory settings, but I believe this would also save all of the HMI settings, including the Autostart timer. Here is another option of doing a factory reset for Basic Panels if the ProSave option gives you trouble: USB Recovery (Reset to factory) Mode for 2nd Generation Basic Panels |
A rating will be well appreciated. |
|
10/17/2024 1:05 PM | |
Joined: 2/17/2020 Last visit: 8/29/2025 Posts: 1251 Rating:
|
Hi again, If you have the original project downloaded to the HMI device, then you can reset the panel to factory settings via USB (as stated in my previous post) to correct the issue. This way, you avoid the connection problem to the panel that you currently have: USB Recovery (Reset to factory) Mode for 2nd Generation Basic Panels |
A rating will be well appreciated. |
|
This contribution was helpful to
1 thankful Users |
Follow us on