6/26/2019 5:29 PM | |
Posts: 3 Rating:
|
Hi, Am also having the same problem with S7414-4H PLC. Even after doing the Factory Reset am getting the Error LED BUS1F. May be a problem with PLC?? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 06/27/2019 11:30:22New subject after splitting |
|
6/29/2019 9:02 PM | |
Joined: 9/27/2006 Last visit: 9/14/2025 Posts: 12408 Rating:
|
Hello RamarRam; You do know that you can communicate with and download to your CPUs over Profibus, if you have an adequate Profibus CP in your Programming PC, or if you use a PC adapter USB as shown in the following discussion: https://support.industry.siemens.com/cs/ww/en/view/82478488 The important point is to select the PG/PC interface parameters correctly. The descriptions of the LEDs' significance is available in the S7-400H system manual, in section 5.3: SIMATIC Fault-tolerant systems S7-400H (V6.0) https://support.industry.siemens.com/cs/ww/en/view/82478488 The LED description is very general, and do not give you information on which specific slave system is giving alarms. It would be important for you to connect to each PLC and retrieve the diagnostic buffer messages from each, to find out what the CPUs are complaining about. You can use the Save As button on the diagnostic buffer page to load the messages to a text file that you can more easily read. If you need help to understand the logged messages, zip them and attache them to this discussion. Hope this helps, Daniel Chartier |
8/31/2021 1:20 PM | |
Joined: 8/21/2014 Last visit: 9/12/2025 Posts: 1087 Rating:
|
Hello Iago Alcântara, Please try to discuss your question in English language. This is an international community and we try to focus on one language. Posting in English will help you to get more response to your question. This is the translation of your question:
Best regards |
My Forum is the place to personalize your profile, |
|
9/1/2021 11:24 AM | |
Posts: 3 Rating:
|
Hello good Morning! Thank you for the tip |
Follow us on