8/17/2023 3:03 AM | |
Joined: 7/25/2017 Last visit: 8/7/2025 Posts: 362 Rating:
|
In TIA18 (Update 1), I can't configure a KP8 (6AV3 688-3AY36-0AX0) such that it works online. When configured as a standard HMI device (catalog\HMI\Simatic Key Panel\KP8 PN\), online the following error occurs: The installed (online) firmware version is not identical with the configured (offline) firmware version. Firmware version: V1.0 Configured firmware version: R01.00.00 I also tried to configure it as a GSD device using the GSD file downloaded here: https://support.industry.siemens.com/cs/document/50710644/ The above is the only GSD file I could find for it. As a GSD device, the following error occurs: The installed (online) firmware version is not identical with the configured (offline) firmware version. Firmware version: V1.0 Configured firmware version: V01.00.00 The controller is a Sinumerik One NCU1750 (6FC5317-5AA00-0AA0 FS:J). Not that it should matter with Profinet devices; it's a 1517F under the hood. Attached are details of the devices. Is this actually a compatible combination? AttachmentKP8 firmware issue.zip (527 Downloads) |
Follow us on