9/20/2023 11:21 AM | |
Joined: 2/3/2022 Last visit: 4/23/2024 Posts: 304 Rating:
|
Hi! Some indication regarding the USB port including in the basic panels manual are the following: - If you connect an external device with a 230 V power supply to the USB port without using a non-insulated installation, you may experience functional problems. Use a non-insulated system design. - A USB device with too high a power load may possibly cause functional problems. Observe the values for the maximum load of the USB interface. You can find the values in the section "USB X60". Br! |
8/1/2025 9:53 AM | |
Joined: 10/16/2018 Last visit: 8/19/2025 Posts: 39 Rating:
|
Hello ThomeFernando13 I also have this same problem, Can you please confirm me how do you solved it, Thank you very much |
8/7/2025 9:31 AM | |
Joined: 8/3/2009 Last visit: 9/2/2025 Posts: 16290 Rating:
|
Hello I think the only you can try on HMI side ist to work with the latest Image (V17.0.0.8): https://support.industry.siemens.com/cs/de/en/view/109825750 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on