6/15/2022 3:28 PM | |
Joined: 3/3/2010 Last visit: 8/26/2025 Posts: 10 Rating:
|
Hello! Logo 12/24RCE, 6ED1052-1MD08-0BA1 Panel KTP700, 6AV2123-2GB03-0AX0 Tia Portal V17 Logo Soft Comfort V8.3 |
6/15/2022 10:22 PM | |
Joined: 3/3/2010 Last visit: 8/26/2025 Posts: 10 Rating:
|
Hi! Basic Module Logo! takes the time sinchronization from GPS (CMR2020 Module) I need this time sinchronized in my HMI |
6/16/2022 8:06 AM | |
Joined: 12/18/2014 Last visit: 9/17/2025 Posts: 35967 Rating:
|
Try this: Make only a connection in TIA, not in LSC. Use the communication driver "SIMATIC S7 200". Only with this driver you have a access to the area pointer. With the communication driver "LOGO!" you can't set area pointers. See attached Screenshot 1. Then select the tab "Area pointer". Go to "Gloabal area pointer of HMI device". There select "Date/time PLC". Use the connection that you before create, enter by address "VW991", by aqcuisition cyle "1 Minute". See attached screenshot 2. In LOGO! is in the VM area the time and the date in hexadecimal at the follow addresses: VB991 = Year VB992 = Month VB993 = Day VB994 = Hours VB995 = Minutes VB996 = Seconds You must nothing do in LSC for the date/time synchronization.
AttachmentScreenshots.zip (518 Downloads) |
Follow us on