12/21/2007 4:21 PM | |
Joined: 1/29/2006 Last visit: 8/16/2025 Posts: 451 Rating:
|
RTFM! |
12/22/2007 9:18 AM | |
Joined: 9/27/2006 Last visit: 9/15/2025 Posts: 12408 Rating:
|
Hello Pacio; Not sure whether this answers your question exactly, but here is a link to a Siemens FAQ that provides a Function to connect a Step 7 program to a Masterdrive: http://support.automation.siemens.com/WW/view/en/20386822 About the reference word, the easiest way to understand it is to use hex values. The range used by Siemens drives is 0-4000 (hex) --> 0-16384 (dec), where: -4000 represents 100% of the parametrized max. speed -2000 represents 50% of the max. parametrized speed -1000 represents 25% of the parametrized max. speed etc... Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 22.12.2007 09:20 |
|
Follow us on