9/3/2008 8:23 AM | |
Posts: 1 Rating:
|
Hello: maybe the will help you . open the attachment use excel. |
4/15/2018 8:00 AM | |
Posts: 15 Rating:
|
Blindly the Atlas Copco air compressors are very good and powerful air compressor. But personally, I use the Industrial Air ILA3606056 for my industry. If you want to know the performance of this compressor I can say many things for it. Shortly I can say it is a very decent air compressor for home, garage or any industrial job applications. It is 60 gallons Single Stage and Cast Iron Twin Cylinder Air Compressor. This compressor has a powerful 3.7-hp induction electric motor which is strongly able to produce 155 psi max of pressure and 13.4 CFM at 40 psi & 11.5 CFM at 90 psi compressed air. This Industrial Air ILA3606056 supports only 208-240V voltage. For more info about this model please you can visit https://bestaircompressorstore.com/industrial-air-compressor-reviews-and-buying-guide-air-compressor-store/ |
Last edited by: Rogar at: 4/15/2018 8:01:34 AM |
|
Follow us on