4/2/2016 6:33 AM | |
Posts: 3 Rating:
|
Hello I have a problem to get access in the SIMATIC panel, when i put the Login: ADMIN, and the password: 100 the password change when click OK and it set ******** in automatic what can i do? i restart the panel HMI, i did an update, i try to solve with win cc flexible 2008 but doesn´t work the simatic panel is tp 177b 6" pn/dp the message error says 260001 you don¨t have insufficient authorization thank¨s ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 4/4/2016 12:53:49 PMNew subject after splitting |
|
4/6/2016 4:52 PM | |
Posts: 8946 Rating:
|
You use the wrong Login. Try "Administrator" and "100" or ask the guy who setup the password. |
4/10/2016 7:17 AM | |
Posts: 3 Rating:
|
i am sorry i can uploap the file extension AttachmentVideo_1460246685.wmv (992 Downloads) |
4/10/2016 7:36 AM | |
Joined: 4/23/2010 Last visit: 11/23/2024 Posts: 8092 Rating:
|
Please check this link. |
5/10/2023 1:04 PM | |
Joined: 11/30/2022 Last visit: 4/20/2024 Posts: 7 Rating:
|
Can i use this way for change my old screen to new model ? |
Follow us on