5/14/2025 9:19 PM | |
Joined: 7/25/2017 Last visit: 9/11/2025 Posts: 362 Rating:
|
I thought that Telegram 112 only works in Isochronous mode - did you get it working with non-Isochronous? |
5/15/2025 6:28 AM | |
Joined: 3/25/2015 Last visit: 8/5/2025 Posts: 124 Rating:
|
Hello, telegram 112 is the same as telegram 111, but it uses REAL values instead of DINT values for MDI setpoint and actual values. EPOS functionality is the same. There's a slight different bit assignment in one of the control/status word, but I don't remember which you can find SINAPOS block and documentation here:
I've also managed to use SinaPara to achieve Fixed End Stop with parameters from PLC instead of fixed traversing blocks in the drive. It's all in the documentation. |
Last edited by: Moderator_Lan at: 05/15/2025 07:46:42link optimized Kind regards |
|
Follow us on