7/25/2007 1:25 PM | |
Posts: 87 Rating:
|
Dear Experts, In my step 7 project I have inserted new Sinamics S120 object (As shown in the attached file) and through that object I can configure it on starter via double clicking it from step 7. After I configure it from Starter, How can I incorporate this object in my step7 hardware manager? I have starter v4.0 and step 7 (PCS 7 v7.0) installed on my PC. I want to put this object into CPU's profibus node. but when I open my hardware manager I can not find this sinamics object which I have already inseted. Ankur AttachmentSINAMICS_STARTER_STEP7.pdf (1053 Downloads) |
7/25/2007 2:08 PM | |
Joined: 10/11/2006 Last visit: 9/8/2025 Posts: 6039 Rating:
|
Hello AMJ. It is not necessary to include a seperate sinamics objekt in the simatic manager. If you do this, then you can´t include your configured sinamcis in the hardware manager. To get a consistent project do the following: 1. start the hardware config and include from the Drive Es Basic catalog the S120 you want to use (S120 310DP or S120 320 DP, ...) to the profibus string per drag and drop 2. configure the S120 with programm version and profibus address 3. save the hardware config and load it to the cpu 4. open your simatic manager and you will find the sinamics located under the cpu (screenshot) 5. double clicking on these object opens starter software and you can configure your drive AttachmentS120_in_simatic_mananger.pdf (1128 Downloads) |
With best regards, |
|
12/6/2007 5:21 PM | |
Posts: 1 Rating:
|
hello i have exactly the same problem with s120 , cu310dp starter and no grive es. a little help would be appreciated. regards |
Follow us on