7/25/2025 4:16 PM | |
Joined: 1/4/2024 Last visit: 9/5/2025 Posts: 15 Rating:
|
Colleagues, good afternoon. I need to configure the Modbus RTU protocol on Siprotek Compact 7SJ80. There is an RS-485 interface. 1. Using Digsi 4 via USB, I connected to the terminal. 2. I created a new project and clicked Divece -> Digsi. Everything was unloaded from the terminal. 3. While in Online mode, I go to the Interface. There I configure Modbus RTU. 4. I click the OK button, open the interface again and the Digsi->Divece button becomes active. 5. I click the button, it loads into the terminal, the terminal reboots. 6. We check Modbus - everything is ok. Now, if I compare projects before and after changing the interface, I get a lot of differences. I can't understand where these differences come from and how critical they are. Below is the list. Attachment7SJ802 V4_8 Var_prn_16_30_16.pdf (144 Downloads) |
Follow us on