2/27/2019 4:55 PM | |
Joined: 2/10/2006 Last visit: 6/2/2025 Posts: 149 Rating:
|
It appears my assessment of the function of this XSUB1 was completely wrong. it doesn't have anything to do with communication to the MP370 panel via RS232 serial connection. When connecting serially to an MP370 HMI panel no XSUB or any special program is needed. This XSUB was used to configure PID loops. This was probably done for performance reasons. in more recent TI545 / TI555 and CTI 2500 CPU's PID Loops are integrated as a standard function and there is no reason to use this XSUB for PID loop execution. To whom it may concern attached is a description of the functioning of this XSUB. I do not recommend to use this for new implementations. Regards, AttachmentFast Loop.pdf (1324 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on