11/26/2024 12:11 PM | |
Joined: 8/17/2019 Last visit: 8/7/2025 Posts: 33 Rating:
|
I bumped into this as we have similar issue. In our setup with two monitors, when the Windows with WinCC starts the first time the monitors are assigned correctly to the functioning of the wincc. The Runtime starts automatically on the start of the computer. When there's no user signed in, the start is triggered by the user signed in. Did anyone find how to control this RDP WinCC interaction so that it provides stable environment for monitor/coordinate system in which we can position the popups etc correctly? ------------------------------------------------------------------------------------------ |
Last edited by: Moderator_Lan at: 11/26/2024 14:01:40New subject after splitting Last edited by: Moderator_Lan at: 11/26/2024 14:02:16Title updated |
|
11/26/2024 3:16 PM | |
Joined: 8/3/2009 Last visit: 9/2/2025 Posts: 16290 Rating:
|
Hello Which WinCC Version do you use exactly? It s because the starter of the topic uses a very old V14 Version, this is not developed any more. Do you use the latest WInCC V19 Upd3 on engineering and RT? Bye Murof |
If this Information really helps, you could use the Rate function |
|
3/31/2025 1:56 PM | |
Joined: 8/17/2019 Last visit: 8/7/2025 Posts: 33 Rating:
|
The WinCC 7.5 is used. |
4/4/2025 8:13 AM | |
Joined: 8/3/2009 Last visit: 9/2/2025 Posts: 16290 Rating:
|
Hello JaSemJa Do you use the latest Update and SP on your WinCC V7.5 There has been a lot of versions for the V7.5... Also if there are troubles with RDP sessions you could also use as an alternative VNC: https://support.industry.siemens.com/cs/de/en/view/78463889 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on