4/14/2025 9:15 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, Welcome to the community When you have a redundant OS server, you have to confgure only one OS project, because both OS projects must be equal. The same OS project is downloaded to both servers. There are however some local settings that must be done, like setting the redundancy options. You won't have to compile the OS server project, because you did not change the CFC logic right? You only changed the User Administrator settings. Normally this change can be done by an OS download change, were both servers are downloaded, first standby then master server. If you have made a lot of changes (a lot of tags), you may end up that download change cannot be done, in this case you need to full download one server, wait for the server to be in runtime and synchronization is complete, and then you full download the other server. In this way, the operator won't loose visualization. For the clients, you can download them one by on from the ES. |
If I could help you, you can use the RATE button. Thank you. |
|
4/15/2025 4:45 AM | |
Joined: 3/14/2008 Last visit: 9/11/2025 Posts: 2216 Rating:
|
Hi, See the following manual for more information about downloading. You can also find which changes can be downloaded with a change and which not. SIMATIC PCS 7 Operator Station (V10.0). See chapter 19 and 20. The OS download change is executed automatically by the system. Both servers will remain in runtime. You won't have to configure anything. If in any case, the downloading fails, you need to execute a full downloiad instead. Synchronization is still active, but when you download full a server, then that server is missing alarms and tags in the period runtime is not active. Therefore, after the server is back in runtime, synchronization occurs so that the returned server is up to date again. You can however stop the second server immediately when the first server is back in runtime when a full download is executed, but this can cause a gap in the alarms and taglogging. Changed in User Administrator are not taken from the server. A change must be done in the client project and then downloaded to the client. PS: You can also import/export the configuration of the User Administrator, so it's easier to use. Also think about using SIMATIC Logon. This allows you to only configure authorization for groups instead of doing this for each person. New users can be added to groups in Windows and they automatically receive the group authorization when logged on to WinCC.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on