5/12/2025 10:54 AM | |
Joined: 10/5/2021 Last visit: 7/14/2025 Posts: 5 Rating:
|
Hello everyone, please explain what this means and what to do about it? A: The number of booked process objects (630) has not changed since the last download. AttachmentArchive.txt (80 Downloads) |
5/12/2025 3:48 PM | |
Joined: 3/14/2008 Last visit: 9/8/2025 Posts: 2216 Rating:
|
Hi, If you configure an object like a VlvL, it costs one AS RT PO. During download the system checks of the new object is booked. The system will take one RT PO from the ES and books to the CPU. The same applies if an PO is deleted. It will book back 1 PO to the ES. If no changes have been made to PO, this message is shown. You can ignore this.. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on