1/30/2024 12:57 PM | |
Joined: 7/19/2022 Last visit: 6/5/2024 Posts: 363 Rating: (61) |
Hello AutoGen_2507851, The S7-410-5H CPU can be used in STEP 7 without the need of PCS7: Operation of CPU 410 in the context of SIMATIC STEP 7 HSP267 v2.0 is required for use in STEP 7 from version V5.6, which is no longer available in SIOS, so you must request it through a technical support request. |
Last edited by: JBS98 at: 01/30/2024 12:58:19Last edited by: JBS98 at: 01/30/2024 12:58:27If this Information really helps, you could use the Rate function |
|
Follow us on