5/7/2020 11:29 AM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating:
|
Hello With OPC XML DA you also have access to SIMOTION variables Information about OPC XML DA: The SIMOTION IT OPC XML DA server enables access via Ethernet to data and operating modes of the SIMOTION controller. As of V4.2, a separate license is no longer required for SIMOTION IT OPC XML DA. OPC stands for open connectivity and refers to standardized software interfaces which enables the exchange of data between applications from different manufacturers in automation technology. With OPC XML DA, it is possible to communicate with a control using Ethernet based standard message frames. Commands are transmitted via the SOAP (Simple Object Access Protocol) communication protocol. A customer-specific application created on a client PC, which, for example, is programmed with the C#, Visual Basic, or Java programming language, uses the SIMOTION IT OPC XML DA services and properties: ● Open communication using HTTP, SOAP, OPC XML between client and SIMOTION device ● Uses the OPC XML DA 1.0 specification of the OPC Foundation ● Access to SIMOTION variables –Reading/writing –Cyclical reading of so-called "subscriptions" –Browsing ● Trace using SOAP; this function is an extension of the OPC specification ● Clients on any hardware with various operating systems (Windows, Linux, etc.) ● Creating client applications using C#, Java, C++. You must implement the application that you want to access on the SIMOTION OPC XML DA server yourself. ● Access protection with user groups, user ID, and password The following figure is a schematic representation of access to the OPC XML DA server. Details: https://support.industry.siemens.com/cs/ww/en/view/109749943 (please note: SIMOTION >= V51. also supports OPC-UA) |
With best regards, |
|
9/26/2022 8:08 AM | |
Joined: 10/11/2006 Last visit: 7/12/2024 Posts: 5874 Rating:
|
http://<IP-Address>/soap/opcxml Details:https://support.industry.siemens.com/cs/ww/en/view/109749943 |
With best regards, |
|
Follow us on