6/21/2013 3:08 PM | |
Joined: 5/12/2011 Last visit: 2/19/2024 Posts: 78 Rating: (1) |
DEAR ALL, 6ES7197-1LA04-0XA0 I AM HAVING THIS Y COUPLER WITH ME, NOW I AM NOT FINDING THIS IN MY HARDWARE CATLOG AND GSD FILE ALSO NOT ABLE TO DOWNLOAD FROM NET. AND ONE MORE DOUBT THROGH THIS PRODUCT WHETEHR I CAN COMMUNICATE S7 400H TO S7 151-7 DP CPU. PLEASE SOMEBODY REPLY..........
|
6/21/2013 3:37 PM | |
Joined: 9/27/2006 Last visit: 4/28/2024 Posts: 12257 Rating: (2665)
|
Hello dhinagaran; There is no need for a gsd file to setup a Y-link if you have a S7-400H redudant master, as you can see in our friend fritz'reply tothis thread: GSD file for Y-Coupler |
Last edited by: O_Moderator at: 6/21/2013 5:40 PM |
|
This contribution was helpful to3 thankful Users |
6/22/2013 1:26 PM | |
Joined: 5/12/2011 Last visit: 2/19/2024 Posts: 78 Rating: (1) |
THANKS FOR HELPING I FINISHED IT. REGARDS V.DHINAGARAN
|
6/23/2013 9:35 PM | |
Posts: 62 Rating: (4) |
Dear dhinagaran, For configuring the Ylink u need not to have the gsd file .but for that u have to select the Y-link compactible IM and select the profibus-dp in it. for more detail please find attached file. Regards, Avinashkrishna Bhimavarapu
AttachmentYlink.zip (358 Downloads) |
Last edited by: Avinashkrishna at: 6/27/2013 11:53 AM |
|
Follow us on