7/23/2015 8:41 AM | |
Joined: 5/22/2010 Last visit: 3/26/2024 Posts: 97 Rating: (2) |
Hello Friends , I am facing a issue in SFC 81 while testing logic with PLCSim. SFC 81 not able to transfer data from Inuput to DB. Kindly suggest. Regards Manish
---------------------------------------------------------------------------------------------------- |
Last edited by: MANISH@TCS at: 7/23/2015 8:48:07 AMLast edited by: Min_Moderator at: 7/23/2015 10:21:47 AMNew subject after splitting |
|
7/23/2015 9:21 AM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Dear User, S7-PLCSIM can not imitate the whole functionality of a real Hardware: What is the difference between S7-PLCSIM and a "real" automation system?and SFC81 is one of the cases.Please test your program with an actual hardware.
hdhosseini |
Last edited by: hdhosseini at: 7/23/2015 9:25:44 AM |
|
This contribution was helpful to1 thankful Users |
7/24/2015 7:47 AM | |
Joined: 5/22/2010 Last visit: 3/26/2024 Posts: 97 Rating: (2) |
Thanks hdhosseini, Right now , I donot have actual hardware, So not able to test. Thanks For your help Regards Manish |
7/24/2015 12:30 PM | |
Joined: 5/22/2010 Last visit: 3/26/2024 Posts: 97 Rating: (2) |
Hi , Can you please tell me , is PLC 414-2DP support SFC81 or not ? Regards Manish |
7/24/2015 12:53 PM | |
Posts: 1058 Rating: (93) |
Hello Manish@TCS, SFC 81 is a standard function for S7 300/400. See here for details: Manual: System Software for S7-300/400 System and Standard Functions Volume 1 and Volume 2 regards |
7/24/2015 1:50 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359)
|
Hello MANISH@TCS , Just to add a small point, the instruction manual for a family of CPUs also provides the list of all supported basic instructions and system functions.For each case, you will find an approximate execution time.For your case, check your CPU , if it is listed in applicable modules.Then have look in page 137: https://support.industry.siemens.com/dl/files/435/23904435/att_89274/v1/OP-Liste_en.pdf another point, if you are not able to test the function, others here can test and upload a snapshot for you. I hope this helps, hdhosseini |
Last edited by: hdhosseini at: 9/2/2015 8:51:52 AM |
|
Follow us on