12/16/2019 7:58 AM | |
Posts: 95 Rating: (0) |
screen shot attached. |
12/17/2019 4:23 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Is it the same problem which is described under Error 2000 plc sign of life monitoring post? I presume here this problem of another machine. Please switch off power machine, first pull out PCMCIA card, then depending upon front plate type, take out main card, clean unit with air blower, clean its PCB connector, refit the main card & plug in PCMCIA card, ensure both are fitted proeprly. Switch ON the power & check if NCU 7 segment displays any digit, dot etc. etc. If it doesnot, you need to get your NCU box check/test. HTH. |
12/17/2019 7:45 AM | |
Posts: 95 Rating: (0) |
sir,this is another milling machien. why this fault occur? what is the root cause? |
12/18/2019 8:52 AM | |
Posts: 95 Rating: (0) |
dear sir, after cleaning its working ok sir. |
This contribution was helpful to1 thankful Users |
Follow us on