Industry Online Support
Technical Forum
3/22/2012 9:56 AM | |
Posts: 376 Rating:
|
Hello AMAZINGAHMED, Unfortunately, I do not have any documentation to the digital input module 6ES5 420-4UA11.Perhaps this information helps you. The new version 6ES5420-4UA12 modules are 100% compatible to the old 6ES5420-4UA11 module. The following feature has been added to the new modules: The enabling input (F+/F-) can be switched off by means of a jumper that is located in the vicinity of the address switch. If the enabling jumper has been removed, the module can be accessed via the S5 backplane bus irrespective of whether the enabling input F+/F- carries a signal or not. It is then no longer mandatory to connect an enabling signal to each module. Concerns products with the Order Nos.:6ES5 420-4UA12, 420 digital input module, previous 6ES5 420-4UA13, 420 digital input module, new Anew digital input module 6ES5 420-4UA13 is now available for SIMATICS5-135U/-155U PLCs. The new module is a revised version of the 6ES5 420-4UA12 module and is fully compatible. Specifications: 32 inputs; input voltage: 24V DC; non isolated. The module replaces the existing version 6ES5 420-4UA12 and is fully compatible. Regards Azteke0110 |
This contribution was helpful to
1 thankful Users |
3/22/2012 10:31 AM | |
Posts: 376 Rating:
|
Hello AMAZINGAHMED, with this Link you find the System manual for SIMATIC S5, S5-135U/S5-155U. In chapter 8 on page 8-30 you finds the specification sheets for the Digital Input modules with the order number 6ES5 420-4UA13and 6ES5 420-4UA14. Unfortunately no information about the 6ES5 420-4UA11. Here the Link for this manual. http://support.automation.siemens.com/WW/view/de/1085837/0/en Regrads Azteke0110 |
Follow us on