6/15/2022 4:28 AM | |
Joined: 10/12/2014 Last visit: 2/27/2024 Posts: 66 Rating:
|
Hello Experts ; Please explain how to tune the Z axis motor in the 802D system. |
6/15/2022 5:25 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Please refer 802D: Turning, Milling manual chapter 3.8 |
6/15/2022 8:31 AM | |
Joined: 10/12/2014 Last visit: 2/27/2024 Posts: 66 Rating:
|
Thank you very much for your support, but I can not find a page for Tune the Axis. |
6/15/2022 10:46 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating:
|
Hello, Please refer chapter Commissioning of above manual which will help you to set related parameters. Please note, you should have SINUMERIK 802D User Documentation − SINUMERIK 802D Description of Functions − A PC for commissioning and data backup − Tools installed from the Toolbox CD: WinPCIN PLC802 Programming Tool SimoCom U Text Manager (is installed using the ”802D Toolbox” menu item) The mechanical and electrical installation of the system must be completed. Starting up the SIMODRIVE 611 UE drive (with the Profibus option module inserted) ready as explained in manual. With help of Sinucom U follow & conduct current, speed, position control loops. Please refer attached sheet which helps you to understand drive optimization procedure with Simucom U in 802D system. Hope this helps. AttachmentDrive Optimization.pdf (249 Downloads) |
This contribution was helpful to
1 thankful Users |
6/15/2022 3:17 PM | |
Joined: 10/17/2007 Last visit: 6/26/2024 Posts: 4007 Rating:
|
Hi, neththi I see PISCEAN already answered you. Now a small reminder. 802D using SIMODRIV 611U, motor turning actually using "SIMO COM U" SW I don't know why you want to "turn" the motor, but make back up by SIMO COM U for the axis you want to turn and save it in good name and copy to another location in you PC or to USB,
|
Last edited by: nulizhang at: 06/15/2022 16:01:08If you like my comments please |
|
6/16/2022 5:12 AM | |
Joined: 10/12/2014 Last visit: 2/27/2024 Posts: 66 Rating:
|
Hellonulizhang ; Thank you for answering, I'm trying to fine-tune the motor after a Contour alarm occurred numerous times while it was running. Br Tharindu |
Follow us on