Industry Online Support
Technical Forum
7/30/2011 11:03 AM | |
Joined: 1/19/2008 Last visit: 4/19/2024 Posts: 980 Rating: (63) |
Hi, If they are standard axes you can do it all in a tool change cycle in the NC. Pee |
8/1/2011 10:39 AM | |
Posts: 38 Rating: (0) |
Hi, Tool change logic should be written in tool change part program. here you can define x & z axis positions directly or with G75. If your magazine is Servo axis you can program in 2 ways (1) Via NC Part program(2) PLC axis control. for NC controlled we need to write part program For PLC axis logic Pls. refer to PLC example file which comes after installing PLC tool box of 802dsl. After installing tool box you will find the description file inyou PC as shown below Start ---> Programs ---> Programming Tool PLC 802D ---> Lib802dsl-->Description English -- In this document you may search for IS_PLC_axis Rantu AttachmentPLC axis_decription.pdf (252 Downloads) |
Follow us on