3/9/2023 11:49 AM | |
Joined: 1/21/2013 Last visit: 6/3/2024 Posts: 2830 Rating: (453) |
Hi luka31, It looks like the web runtime is not running. Can you please provide more information? What image version is being used on the device? Is Update 5 already installed? Please also try using the V18 image on the Comfort Panel without changing the project. Kind regards |
3/10/2023 8:26 AM | |
Joined: 4/3/2017 Last visit: 5/15/2024 Posts: 69 Rating: (1) |
I downloaded update 5, but the result is the same. I don't have TIA v18. Is it necessary to have TIA 18 to be able to use panel image v18? The information about the panel is in the attached image. |
Follow us on