Industry Online Support
Technical Forum
11/12/2013 3:10 PM | |
Posts: 220 Rating: (11) |
Hi Engr-Trainee Maybe this two Links will help you:
|
11/12/2013 9:17 PM | |
Joined: 3/14/2008 Last visit: 5/31/2024 Posts: 2070 Rating: (928) |
Maybe it is an option to use Advanced ES... You can import data from PCS7, use your own created excel sheets or those from the supplier and make a configuration. The configuration could be process tag based (only process tags), signal (defining IO addresses) or both.. When your done with your configuration, you can import the excel data and then all your control modules (CFC charts with your logic) will be created... Then you export the data to PCS7 and voila, plant ready (sort of speak). you can even assign which SM modules and IM modules you want to use with the mlfb number.. When exporting, ET200 modules with IO modules are automatically created in your hardware AS!!! |
If I could help you, you can use the RATE button. Thank you. |
|
11/13/2013 10:06 AM | |
Posts: 220 Rating: (11) |
More Informations to AdvES and how to use it find youhere. |
Follow us on