5/25/2023 5:03 PM | |
Joined: 8/3/2022 Last visit: 5/27/2023 Posts: 3 Rating:
|
Hello, I have issue with analog bar - cannot retentive value from the bar. After power on value is 0. On the animation settings this bar can be 15 minimum and 24 maximum. Blok type VW. When I set this bar once the only value with can be is from 15 to 24 (what is ok ) but after logo start and i do not touch bar the value is 0. Any ideas ? Regards Peter AttachmentAnalog bar.zip (621 Downloads) |
5/26/2023 3:50 PM | |
Joined: 12/18/2014 Last visit: 9/15/2025 Posts: 35964 Rating:
|
The same ask you in this topic: Analog bar retentive for power failure or stop modePlease don't post twice for the same problem. |
This contribution was helpful to
1 thankful Users |
5/30/2023 8:12 AM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8171 Rating:
|
Closed cause question posted twice. The second thread with the subject Analog bar retentive for power failure or stop mode is published within the conference LOGO! - Software. Best regards, |
Follow us on