12/20/2021 4:43 PM | |
Joined: 4/15/2014 Last visit: 1/9/2024 Posts: 16 Rating: (3) |
Hello David, did you find the problem at the end? I'm having the same issue, and axis wh should move at 2500 mm/sec but moves at 250mm/sec, (in the "limits" section I have 3000 mm/sec so they are not the problem). ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/21/2021 10:10:38New subject after splitting |
|
12/21/2021 5:25 PM | |
Joined: 7/7/2010 Last visit: 10/7/2024 Posts: 15270 Rating: (2422) |
Is this in job movement, or normal automatic motion? job motion is defined to be slower. Is it possible there is a scaling thing going on where there is an "implied" decimal where 2500 really means 250.0 (or 250,0 for some regions)?
|
science guy |
|
Follow us on