1/30/2024 12:22 PM | |
Joined: 5/6/2022 Last visit: 5/23/2024 Posts: 420 Rating: (83) |
Hi What I recommend is that to make a backup, it is best that you configure the backup when creating the file. As indicated in the following link: "SIMATIC HMI WinCC Unified Engineering V18: Creating a data log and an alarm log" And then, to restore it later, you can check this link: "SIMATIC HMI WinCC Unified Engineering V18: Restoring and deleting log segments" I hope this information can be of help to you. Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
2/1/2024 11:23 AM | |
Joined: 3/16/2020 Last visit: 5/28/2024 Posts: 9 Rating: (0) |
You are right! Thanks! |
Follow us on