4/24/2010 8:35 AM | |
Posts: 14 Rating: (0) |
Hello: |
Last edited by: O_Moderator at: 4/26/2010 1:34 PMnew subject after splitting Last edited by: shr4plc at: 4/24/2010 8:46 AMLast edited by: shr4plc at: 4/24/2010 8:38 AM |
|
4/24/2010 10:56 AM | |
Joined: 10/7/2005 Last visit: 6/18/2024 Posts: 3008 Rating: (1051)
|
Hello shr4plc [schnippschnapp]
You can, but not via the same Profibus port (e.g. you need two DP ports anda CP342-5 is a good way to get additional DP ports if your CPU has only oneonboard). I hope this helps |
Last edited by: O_Moderator at: 4/26/2010 1:36 PMCheers |
|
4/24/2010 1:45 PM | |
Posts: 14 Rating: (0) |
my CPU is 313C-2DP. on PORT DP is written "×2DP". what is that mean ? |
4/24/2010 2:32 PM | |
Joined: 10/7/2005 Last visit: 6/18/2024 Posts: 3008 Rating: (1051)
|
Hello again shr4plc I must admit it never occured to me that the "×2DP" naming can actually be confusingand leadpeople to (falsely) assume that this port canfor example have two DP functionalities at the same time (e.g. being a DP Master and DP Slave at the same time). Unfortunately the "×2" simply means that this is the second onboard port/interface (the "×1" is the first one and is in your case an MPI port that can NOT be changed to act as a DP port). Just to be clear: The "×2DP" port can be configured to be either a DP Master OR a DP Slave, but NOT both together (well, if you configure it as a DP Slave and also tick "Test, commissioning, routing", it will also assume a Class 2 DP Master role to allow routing and speed up online access, but this is NOT whatyou are after, so please do not get confused by this rather superfluous technical detail). I hope this helps |
Last edited by: fritz at: 4/24/2010 2:43 PMCheers |
|
This contribution was helpful to2 thankful Users |
10/10/2013 1:20 PM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2682 Rating: (135) |
New question splitted to make IM151 as SLAVE to 317 plc and MASTER to Drive Best regards O_Moderator |
Follow us on