10/10/2013 6:44 AM | |
Joined: 10/7/2005 Last visit: 8/9/2024 Posts: 3016 Rating: (1054)
|
Hello naveen_paliwal yes it can, but you willin thecase ofits PN port usagehave to go forthe so called "Open Ethernet communications"and handle the connection establishment via your user program instead of via NetPro. Have a look at What are the commonalities and differences between configured communication connections and the open Ethernet communication? for more on this (and note the links to the examples) as well as the CPU-CPU Communication with SIMATIC Controllers compendium which is an excellent reference source on that matter. I hope this helps |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on