9/11/2011 8:29 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello, Please attach here your sample project. best regards, Hristo MIhalev |
9/16/2011 10:10 AM | |
Posts: 103 Rating:
|
hi.... umencho i m here sending uthe my project take a lookon it i want to tell u that when i try to run this in plc its lmn ,error value do not get any change, pls find the attachment Attachmenttest_pid.zip (608 Downloads) |
9/16/2011 11:00 AM | |
Joined: 1/28/2009 Last visit: 9/15/2025 Posts: 6875 Rating:
|
Dear veer Please refer to the following Tag in which 2 threads clustered. Those threads are about sample example projects to handle FB41. Standard PID Package - FB41 Samples The following points are strange for me: 1- small integration time of 100ms 2- using the whole block as a P controller by disabling I and D parts You have constant error signal because you are using a P controller in which error=P*(SP-PV) Also check the attachment for the online help of the function. Best regards Attachment1.pdf (1213 Downloads) |
9/16/2011 2:04 PM | |
Posts: 103 Rating:
|
hi... marc if i didnt define pv_per this means not that i dont get lmn and i wanna tell u that this program run proprly in plc sim so why dont same action in actual plc. and also take look on this atttachment which shows area length error AttachmentDiagnose.zip (497 Downloads) |
9/16/2011 3:36 PM | |
Joined: 1/28/2009 Last visit: 9/15/2025 Posts: 6875 Rating:
|
Hello again Please Note, you have problem in other FBs inside your project.To check FB41,just check the following modified version of your program.Besides, you need to change SP_INT,I also include it in your project,add I part to your algorithm and change the integration time to 10s. Best regards AttachmentMODIFIED.zip (594 Downloads) |
Last edited by: hdhosseini at: 9/16/2011 3:38 PM |
|
Follow us on