3/25/2020 8:38 AM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating:
|
Hi, I installed pcs7 v8.2 and see the check mark 4 in the faceplate of the ConPerMon block in the Limit view window of the attached file, while message suppression is not active either on the faceplate or on the block bases (MsgLock Parameter = 0) Also I don't have any alarms in, message list Does anyone know how to turn it off? Because the manual refers to the xx_MsgEn parameter which is not such a block in the I/O tab at the base of the block. AttachmentImages.zip (34 Downloads) |
Last edited by: amirab at: 03/25/2020 08:39:15 |
|
3/25/2020 10:22 AM | |
Joined: 9/3/2013 Last visit: 11/3/2023 Posts: 152 Rating:
|
The Manual refers also to other inputs. https://support.industry.siemens.com/cs/de/en/view/109739941 e.g. CPI_WL_En or CPI_Suppress you should check these also. The parameters "xx_MsgEn" are a part of the status words. See chapter 4.2.1 Regards |
3/25/2020 2:51 PM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating:
|
Hi Technodrome As shown in figure 2, bit 15 of status1 is related to CPI_Suppress which is equal to 1 in my program as shown in figure 1, my question is how is bit 1 done? Because I did not enable message suppress on the corresponding faceplate and I did not set MsgLock on cfc. Best regard AttachmentImages.zip (34 Downloads) |
Follow us on